AXIS#.MOTOR.TBRAKERLS

Description

This parameter is used to configure the mechanical delay when releasing the motor brake. AXIS#.MOTOR.TBRAKERLS is a time delay that is applied when a brake exists and the drive is enabled. When the drive is enabled, the brake is commanded to release and, during the AXIS#.MOTOR.TBRAKERLS period of time, the drive does not accept a motion command. This delay allows the brake to fully release before the drive begins a new motion.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms 

Range

0 to 1,000 ms

Default Value

75 ms
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
AXIS1.MOTOR.TBRAKERLS

500bh

1bh

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.TBRAKERLS

510bh

1bh

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TBRAKERLS

6216

1848

Unsigned16

Read Only

-

AXIS2.MOTOR.TBRAKERLS

71752

1184

Unsigned16

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TBRAKERLS

6216

Unsigned16

Read Only

-